STMicroelectronics and NUS launch Corporate Lab to power the future of Edge AI in Singapore
STMicroelectronics and NUS launch Corporate Lab
to power the future of Edge AI in Singapore
- HELIX joint R&D initiative to enable new generative and embodied AI use cases at the edge through system-to-silicon innovation
- Research will focus on memory-centric architectures, innovative in-memory computing, scalable compute-and-memory systems, and advanced silicon and embedded-memory technologies
- Corporate Lab will strengthen Singapore’s advanced semiconductor research capabilities and support the development of future edge AI talent and innovation
Singapore, 24 August 2026 – STMicroelectronics N.V. (“ST”) (NYSE: STM), a global semiconductor leader serving customers across the spectrum of electronics applications, and the National University of Singapore (NUS) have officially launched the ST–NUS HELIX Corporate Lab, a four-year strategic research initiative focused on advancing the next generation of edge AI technologies. HELIX, which stands for Hardware for Embodied Low-power Intelligent Xcceleration, will enable new generative and embodied AI use cases at the edge through system-to-silicon innovation.
The Corporate Lab is supported under the Research, Innovation and Enterprise 2025 plan (RIE2025) and is hosted at the College of Design and Engineering and with participation from the School of Computing at NUS. The Corporate Lab brings together a multidisciplinary research ecosystem spanning AI algorithms, accelerator architectures, low-power memory systems, circuit design, silicon technologies, and application development. The programme will integrate NUS’ pioneering research with ST’s expertise in semiconductor technology, system development, and industry operations.
NUS President Professor Tan Eng Chye said: “The ST–NUS HELIX Corporate Lab is a testament to the value of industry–academia partnerships in translating research into innovation. By combining NUS’ research strengths with STMicroelectronics’ industrial capabilities, we are building not only advanced, cutting-edge edge AI hardware, but also the talent and ecosystem that will help define the future of Singapore’s semiconductor and AI industries.”
Laurent Malier, Executive Vice President, Global Technology R&D at STMicroelectronics, said: “ST’s strength as an integrated device manufacturer lies in our ability to bring together advanced silicon technologies, embedded memory, circuit design, heterogeneous integration and chiplets. Through HELIX, we are creating an industrially relevant foundation to explore differentiated AI computing technologies and accelerate the translation of promising research into scalable semiconductor solutions.”
The Corporate Lab was officially launched today by Ms Low Yen Ling, Senior Minister of State, Ministry of Culture, Community and Youth, and Ministry of Trade and Industry, as the Guest-of-Honour.
Building the future of edge AI
Edge AI processes data directly within or close to a device rather than relying exclusively on remote cloud infrastructure. This enables faster response times, stronger data privacy, improved energy efficiency, and greater resilience in environments with limited or intermittent connectivity. These capabilities are increasingly important for AI systems that must perceive, reason, and act in real time, in the real world – often described as Physical AI.
HELIX focuses on a key frontier within this space: embodied AI, where intelligence is built directly into a physical form — such as a robot, humanoid, or drone — combining multi-modal sensing, on-device computing, and real-time actuation. Delivering that intelligence efficiently, on compact and power-constrained hardware, is the challenge HELIX is built to address. Enabling these capabilities at the edge requires innovation across algorithms, software, system architecture, and hardware.
HELIX builds on ST’s long-standing journey in AI and will help explore new system-level solutions that combine efficient computing, advanced memory architecture, and application-driven design to address the requirements of future intelligent devices. Complementing ST’s capabilities, NUS brings world-class expertise in integrated circuits, computer architecture, AI models, and system design. Under the partnership, researchers from NUS and STMicroelectronics will jointly work on research work packages, talent development, IP creation, and demonstration activities.
The research at HELIX will span the full technology stack, from AI models and system architecture to heterogeneous accelerators, on-chip memory hierarchies, circuit design, chip integration, and silicon implementation. It will focus on memory-centric architecture, innovative in-memory computing, and scalable compute-and-memory systems, supported by ST’s P18 18nm Fully Depleted Silicon On Insulator (FD-SOI) technology and embedded Phase Change Memory (PCM). P18 FD-SOI enables ultra-low-power operation and adaptive body-biasing, while embedded PCM provides dense, non-volatile storage on the same die alongside the on-chip SRAM hierarchy. Together, these capabilities can reduce the off-chip data movement that dominates the energy consumption of memory-bound AI workloads.
ST will make a substantial technology and engineering contribution to HELIX by providing NUS with a dedicated design chassis implemented in its proprietary P18 18nm FD-SOI technology. The platform will bring together ST’s silicon, architecture, integration, and engineering capabilities to give researchers an industrial-grade foundation for developing, integrating, and validating new AI accelerator concepts. By eliminating the need to build the underlying infrastructure from the ground up, the design chassis will enable greater focus on differentiated innovation, accelerate system-level validation, and create a more direct path from technology pathfinding to industrialization.
By combining advances across AI algorithms, accelerator architectures, memory systems, circuits, and semiconductor technologies, HELIX aims to address the energy-efficiency, memory-bandwidth, latency, scalability, and integration challenges associated with deploying increasingly capable AI systems at the edge.
Nurturing talent to drive Singapore’s semiconductor ecosystem
The establishment of HELIX represents a strategic investment in Singapore’s future competitiveness in edge AI and advanced semiconductor systems. By fostering industry-relevant R&D, HELIX will strengthen local capabilities and nurture a new generation of talent in AI systems and chip design.
Students, researchers, and professionals will have opportunities to participate in cutting-edge projects led by HELIX, gaining hands-on experience with the latest technologies, collaborating with industry leaders, and developing skills that meet the evolving needs of the sector. Through these initiatives, HELIX aims to build a robust talent pipeline and position Singapore as a global hub for innovation in edge AI and semiconductor technologies.
For media enquiries, please contact:
Fun YIP
Office of University Communications
National University of Singapore
DID: +65 6516 1374
Email: fun.yip@nus.edu.sg
Dennis TAN
Integrated Marketing & Communications
STMicroelectronics
Tel: +65 6216 5000
Email: wddennis.tan@st.com
About National University of Singapore (NUS)
The National University of Singapore (NUS) is Singapore’s flagship university, which offers a global approach to education, research and entrepreneurship, with a focus on Asian perspectives and expertise. We have 15 colleges, faculties and schools across three campuses in Singapore, with more than 40,000 students from 100 countries enriching our vibrant and diverse campus community. We have also established more than 20 NUS Overseas Colleges entrepreneurial hubs around the world.
Our multidisciplinary and real-world approach to education, research and entrepreneurship enables us to work closely with industry, governments and academia to address crucial and complex issues relevant to Asia and the world. Researchers in our faculties, research centres of excellence, corporate labs and more than 30 university-level research institutes focus on themes that include energy; environmental and urban sustainability; treatment and prevention of diseases; active ageing; advanced materials; risk management and resilience of financial systems; Asian studies; and Smart Nation capabilities such as artificial intelligence, data science, operations research and cybersecurity.
For more information on NUS, please visit nus.edu.sg.
About STMicroelectronics
At ST, we are 49,000 creators and makers of semiconductor technologies mastering the semiconductor supply chain with state-of-the-art manufacturing facilities. An integrated device manufacturer, we work with more than 200,000 customers and thousands of partners to design and build products, solutions, and ecosystems that address their challenges and opportunities, and the need to support a more sustainable world. Our technologies enable smarter mobility, more efficient power and energy management, and the wide-scale deployment of cloud-connected autonomous things. We are on track to be carbon neutral in all direct and indirect emissions (scopes 1 and 2), product transportation, business travel, and employee commuting emissions (our scope 3 focus), and to achieve our 100% renewable electricity sourcing goal by the end of 2027.
Further information can be found at https://www.st.com
Attachment